Unitree Robotics is a world-renowned civilian robotics company, which is focusing on the R&D, production, and sales of consumer and industry-class high-performance general-purpose legged and humanoid robots, six-axis manipulators, and so on.Unitree Robotics has been invited to attend the 2021 CCTV Spring Festival Gala, the opening ceremony of Winter Games 2022, the 2023 Super Bowl, The 19th Asian Games and The 4th Asian Para Games, and the 2025 Year of the Snake CCTV Spring Festival Gala, and has been interviewed and reported by CCTV and other well-known media for many times.Unitree Robotics is the world‘s first company to start public retail of high-performance quadruped robots, and the first to achieve industry landing, with global sales leading over the years.

Unitree has excellent leadership in core robot parts, motion control, robot sensing and other comprehensive fields.

Unitree attaches great importance to independent research and development and technological innovation, fully self-researching key core robot components such as motors, reducers, controllers, LIDAR and high-performance perception and motion control algorithms, integrating the entire robotics industry chain, and reaching global technological leadership in the field of quadruped robots. At present, more than 200 domestic and foreign patent applications have been submitted, including more than 180 authorized patents.

Cultural Concept

Vision of Unitree:

Technology drives world progress.

Mission of Unitree:

To plant the science and technology tree of the world.

Culture of Unitree:

Ultimate insight, self-achievement, cooperation and mutual benefits.

Strategy of Action:

Always be alert, grasp core logic, set key goals, craftsmanship, be perfect, build the future.

Action Guide:

Subdivision of objectives, efficient execution, proofreading of results, feedback and communication.

Social Contributions

Unitree Robotics brings important contributions to the society through constantly innovative technologies and a wide range of applications. From the 2021 CCTV Spring Festival Gala in the Year of the Ox and the 2022 Winter Olympics Opening Ceremony to the 2023 Super Bowl pre-game show to the 2023 Asian Games in Hangzhou and the Asian Para Games, Unitree Robotics continues to deliver innovative experiences for consumers and professional users.

Since 2017, Unitree Robotics has been committed to promoting the application of high-performance general-purpose footed/humanoid robots in different industries. These robots have been widely used in agriculture and industry, as well as in key areas such as power inspection, survey and exploration, and public rescue, providing strong support for social development.

Human beings may be the passers-by of the universe, but science and technology must be eternal.

The beautiful things are very appealing, but the whole industry has rarely changed the status quo and has been imitating, but this is not our goal. We firmly believe that innovation is the cornerstone of enterprise development and look forward to working together with every like-minded person! In recent years, Unitree Robotics has continued to enrich its product line, improve its product performance, continue to promote the construction and improvement of its existing production line, deeply tap into the market of quadruped robot racetrack ToB and ToC, and at the same time, after a multi-dimensional growth path, Currently, Unitree has covered the fields of consumer-grade and industry-grade high-performance general-purpose legged/humanoid robots and dexterous robotic arms, making people's work and life more convenient, comfortable, and efficient. Unitree Robotics always firmly believes that to become a leader in a subdivided industry and drive the high-quality development of the entire industry is the mission entrusted to each of us by the times! We look forward to starting a new journey of "technology promote the world" with the strength of the group! This is a road that is more and more not lonely, but more and more stable. Because of the development of science and technology, the technology that was out of reach has already entered the homes of ordinary people. We want to keep the beauty of each day in our lives, and we want to use the needs of people's livelihood to light up one human science and technology tree after another!

Year of 2025

On January 28, sixteen H1 humanoid robots from Unitree captivated the audience with their performance of "YangBot" at the China Media Group's Snake Year Spring Festival Gala. Directed by Zhang Yimou, the act seamlessly blended technology with folk traditions, creating a moment where futurism meets heritage. Following its broadcast, the performance transcended cultural boundaries, sparking a nationwide wave of technological enthusiasm.

On May 25, Unitree hosted the world’s first humanoid robot combat competition based on its G1 humanoid robot — marking a new milestone in human history.

On July 25, Unitree released the intelligent companion — the humanoid robot R1. Ultra-lightweight and fully customizable at around 25 kg, R1 integrates voice and images large multimodal models, accelerating the arrival of the intelligent agent era.

On August 5, Unitree launched the quadruped robot A2, weighing around 37 kg. It can walk continuously for 3 hours (12.5 km) with full load, and 5 hours (20 km) without load — lighter, faster, and stronger, redefining a new paradigm for industry applications.

From August 14 to 17, the first World Humanoid Robot Games were successfully held in Beijing. Unitree won four gold medals (1500 m, 400 m, 100 m obstacle race, and 4×100 m relay), ranking first in both the gold and overall medal tallies. The Unitree H1 achieved a top speed of 5+ m/s. In addition, independent teams using Unitree’s G1 hardware platform won 1 gold, 1 silver, and 1 bronze medal.

On October 20, Unitree unveiled the H2 humanoid robot — standing 180 cm tall and weighing 70 kg, equipped with bionic dual-eye cameras and a bionic face, designed to serve people safely and with friendliness.

2024

2023

2022

2021

2020

2019

2017

2016

2016-2013

  • Company Profile

  • Cultural Concept

  • Social Contributions

  • Message from the Founder

  • Company Development